Market News
Vishay Intertechnology's Inductors Division
Earns
ISO
13485:2003
Certification for Yankton, S.D., Facility
Jan 26, 2012
Vishay Intertechnology, Inc. (NYSE: VSH) today announced that the company's Inductors Division has earned the International Organization for Standardization (ISO) 13485:2003 certification for its Yankton, S.D., facility. Vishay's ISO 13485:2003 registration audit was conducted by UL DQS Inc., and the site was certified for the "design, development, and manufacture of inductors, transformers, and antennas for use in medical devices in accordance with customer requirements."
TE Connectivity: Best features of bimetal breaker, PPTC device
protect
battery-based tools
Jan 13, 2012
TE Circuit Protection was honored with an Electronic Products’ 2011 Product of the Year Award for its MHP30-36 product. The MHP (metal hybrid PPTC) device incorporates the best features of a bimetal breaker and PPTC and allows the PPTC technology to be used in higher current applications.
NXP Wins Recognition for Excellence in High Performance Mixed Signal
Products
Jan 03, 2012
NXP USB microcontrollers and JenNET-IP recognized in 2011 EDN Hot 100; EDN China Innovation Awards go to GreenChip SSL driver IC and LCD microcontroller
Semicon industry cuts inventory
Dec 28, 2011
According to IHS Inc., stockpiles from semiconductor suppliers fell in Q3, ending inventory accumulation for the last consecutive seven quarters. The industry went into self-correction mode in order to reduce oversupply, bringing the stockpiles Q3 at 81 days, down 2.5 percent from 83 days in Q2, as calculated by the Days of Inventory (DO I) measure. [EETimes Asia]
Smart meters to boost IC sales
Dec 28, 2011
IHS Inc. has released the details of its research that describes a vibrant forecast for ICs used in smart meters. According to the market intelligence firm, power utilities are seen to adopt smart electricity meters due to their capacity to improve electrical grids efficiency and to save energy. As such, global smart meter shipments will top 62 million units in 2016, up from 20.5 million this year. [EDN Asia]